Part Number: CC2540
Other Parts Discussed in Thread: CC2541
Hi Team,
My customer is designing a USB Dongle and need to confirm if the CC2540 supports the following requirements:
-
Dual Mode Switching: Can the chip support switching between Standard BLE and Proprietary 2.4GHz modes?
-
Proprietary Mode with USB HID: In Proprietary mode, can it function as a USB Mouse/Keyboard while also accepting configuration settings from the PC (bidirectional USB HID)?
If the CC2540 is not suitable for this application, please recommend another single-chip solution that includes BLE, Proprietary 2.4GHz, and a hardware USB interface.
Best regards,