This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1: CC2745R10-Q1 – OSAL usage before vTaskStartScheduler() and without BLE Stack.

Part Number: CC2745R10-Q1

Hello TI Team,

I am developing a custom CAN/UDS bootloader for the CC2745R10-Q1 device using FreeRTOS and ICall/OSAL.

My current flow is:

  • Board_init()

  • ICall_init()

  • ICall_createRemoteTasks()

  • Boot decision logic

  • vTaskStartScheduler()

In the boot decision stage (before calling vTaskStartScheduler()), I attempted to use OSAL APIs such as:

user_osal_Read()
user_osal_Write()

However, these APIs do not function correctly(Hang and not getting control upto terminate the debug session) before the scheduler is started. Once vTaskStartScheduler() is called and the APIs are used inside a task context, they work as expected.


I would like clarification on the following:

  1. Is it expected behavior that OSAL APIs cannot be used before vTaskStartScheduler()?

  2. Does OSAL strictly require a FreeRTOS task context to operate?

  3. Is OSAL tightly coupled with the BLE stack, or can it be used independently?

  4. Can OSAL be used without enabling or running the BLE stack?

  5. For a bootloader use case (no BLE functionality required), what is the recommended method to access NVM services before scheduler start?

  6. Is there a TI-recommended bootloader architecture for CC27xx devices when using ICall/OSAL without BLE?

My objective is to:

  • Perform boot decision (jump to application or stay in boot)

  • Use OSAL-based NVM storage if possible

  • Avoid enabling the BLE stack in the bootloader

for your reference Boot manager main():

unsigned char osal_ret_val = 0;
int main(void)
 {
       pthread_t thread;
       pthread_attr_t attrs;
       struct sched_param priParam;
       int retc;
       int uds_schedular;
       uint32_t reloadValue =0;
       Watchdog_Handle watchdogHandle;
       unsigned char main_eeprom_read[4] = {0};
       unsigned char main_eeprom_clear[2] = {0x00,0x00};
       unsigned char main_eeprom_read_1[2] = {0xA5,0x02};
       unsigned char main_eeprom_read_test[4] = {0};
       unsigned char Security_timer_enable[2] = {0};

 

       /* Register Application callback to trap asserts raised in the Stack */
         halAssertCback = AssertHandler;
         RegisterAssertCback(AssertHandler);


         /* initialize the system locks */
           Board_init(); //initialization of clock and peripherals.
           /* Update User Configuration of the stack */
             user0Cfg.appServiceInfo->timerTickPeriod = ICall_getTickPeriod();
             user0Cfg.appServiceInfo->timerMaxMillisecond  = ICall_getMaxMSecs();

             /* Initialize all applications tasks */
             //appMain();
             /* Initialize ICall module */
             ICall_init();

             /* Start tasks of external images - Priority 5 */
             ICall_createRemoteTasks();


               CheckAndClearResetCause(); //Reset reason.
               /* Watch dog initialization*/
               watchdog_initialization();
               
    osal_ret_val = osal_snv_read(e_JUMP_FROM_APPLN_FLAG_FOR_BOOT_ID, e_JUMP_FROM_APPLN_FLAG_FOR_BOOT_LEN, main_eeprom_read);
    

               
               
               
               if(main_eeprom_read[0] == 0xA5) /* if jump from application //0xA5*/
               {   
                   osal_ret_val = osal_snv_write(e_JUMP_FROM_APPLN_FLAG_FOR_BOOT_ID,e_JUMP_FROM_APPLN_FLAG_FOR_BOOT_LEN,main_eeprom_clear);
                   INIT_BOOT();
               }
               else
               {
                   MCAL_JUMP_To_Appln();
               }
               Software_Timer_Init(); //software timer initialization

              xTaskCreate(CanTp_Scheduler_Task, "CanTp_Scheduler_Task", STACK_SIZE, NULL, 4, NULL);
              xTaskCreate(uds_scheduler_task, "uds_scheduler_task", STACK_SIZE, NULL, 3, NULL);

              MCAL_BOOT_Entry();

              /* Start the FreeRTOS scheduler */
                     vTaskStartScheduler();
   return 0;
 }

I would appreciate guidance on the correct architectural approach.

  • Hello, 

    First, can you provide the SDK version you are using? 

    1. I believe this is a yes. You can see an example here, where the osal functions are called after the vTaskStartScheduler() function has been executed. 

    I apologize for the delay, but I will get back to you next week with answers to the other questions. Please expect a reply Tuesday (03/10). 

    Thanks,
    Isaac

  • Hi,

    SDK version: - simplelink_lowpower_f3_sdk_9_12_00_19.

  • Hello,

    Is it expected behavior that OSAL APIs cannot be used before vTaskStartScheduler()?

    Yes. OSAL stands for Operating System Abstraction Layer, and serve as an abstraction layer for the underlying RTOS. In this case, since you're using FreeRTOS the scheduler will need to be started before the use of these APIs.

    Does OSAL strictly require a FreeRTOS task context to operate?

    Yes. Even if you were to use something like POSIX threads (which are a wrapper around FreeRTOS) it will still use FreeRTOS.

    Can OSAL be used without enabling or running the BLE stack?

    It should be able to be used as long as FreeRTOS is running on the system. 

    For a bootloader use case (no BLE functionality required), what is the recommended method to access NVM services before scheduler start?

    The NVS driver. NVS.h File Reference

    Is there a TI-recommended bootloader architecture for CC27xx devices when using ICall/OSAL without BLE?

    No. I'm not quite sure why you would want ICall or OSAL in a bootloader since those consume a lot of flash. Typically bootloaders are lightweight with no RTOS. 

    Can you give me some more information on what you're trying to achieve with your bootloader? I can provide some better support then.

    Best,

    Nima Behmanesh