Part Number: CC2755P10
Other Parts Discussed in Thread: CC2652P7,
Hi,
I am wondering if the Low Power F3 SDK supports the Periodic Advertisement with responses ?
In the file "C:\ti\simplelink_lowpower_f3_sdk_9_14_02_16\docs\rcl\source\handlers\ble_handlers\periodic_scan_handler.md", I see
"Periodic Advertising with Responses (PAwR) was introduced in Bluetooth Core Specification 5.4 to enable bi-directional communication between an advertiser and multiple scanners within a structured time frame. Unlike standard periodic advertising, PAwR allows devices to send responses within pre-defined response slots, enabling efficient communication while maintaining low power consumption."
If it is supported can you provide an example for the CC2755P10 ? If yes when can I expect this to be implemented in the SDK. Will that be supported on the CC2652P7? Do you have an example for CC2652P7?