Part Number: CC2745R10-Q1
Hi team,
My customer ask some questions about flash size. Please help clarify. Thank you.
1. From CC2745R10 datasheet, Flash size is 1MB. However, the .map file only show length "0XE500" as below which is only 937KB. Are the remaining regions reserved for what kind of application ? (eg. CCFG, SCFG etc.)
OUTPUT FILE NAME: <car_node.out>
ENTRY POINT SYMBOL: "resetISR" address: 00048ccf
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
FLASH 00000000 000e5000 000569b5 0008e64b R X
NVS_SLOT 000e5000 00003000 00003000 00000000 R X
SRAM 20000000 00028800 000165c8 00012238 RW X
S2RRAM 40098000 00001000 00000000 00001000 RW
CCFG 4e020000 00000800 00000800 00000000 R
SCFG 4e040000 00000400 00000400 00000000 R
LOG_DATA 90000000 00040000 00000000 00040000 R
LOG_PTR 94000008 00040000 00000000 00040000 R
2. For the example of car_node project, it uses 345KB (0x0x569B5 as above). If customer want to use A/B partition for OTA. Are the remaining flash space is enough for below items ?
- Bootloader
- Dual image (A/B)
- OTA relating data (eg. Metadata)