Part Number: CC2745P10-Q1
Other Parts Discussed in Thread: SYSCONFIG
I'm trying to update from SDK simplelink_lowpower_f3_sdk_9_10_00_83 to simplelink_lowpower_f3_sdk_9_14_02_16.
SysConfig has also been updated from version 1.23.1 to 1.23.2, and I have confirmed that two new settings have been added to PSA Crypt + KeyStore.

When I opened SysConfig in version 1.23.2, "KeyStore Flash Address Offset" was set to 0xE6000, and building with this setting resulted in an error.
"The configured KeyStore flash region goes beyond the accessible flash addresses on the device."
I have a question about "KeyStore Flash Address Offset" setting.
If the ITS area is set to 32KB starting at 0x000E0000, and the KeyStore Flash Size is set to 10KB, where will the KeyStore area be placed in SDK 9.10?
Also, if I want to maintain the same map as 9.10 after updating to 9.14, what value should I set for "KeyStore Flash Address Offset"?