This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Capture RSSI based on CC2642

Part Number: CC2642R

TI Official Engineer
Dear Sir/Madam,
I noticed the official demo is based on the rtls_coordinator project. I would like to consult whether the connection between my simple_peripheral device and mobile phone can be captured and monitored by Connection Monitor.
Best regards,
Deng Junjie
  • Hello Deng Junjie,

    When running the connection monitor you will need to extract the connection parameters via BLE after the connection event, and then have the CM use those parameters to then monitor/log the connection.

    If your question is just about RSSI on the CC2642R side that should be pretty straightforward to find. 

    Thanks,
    Alex F 

  • Hello, I need to confirm whether the connection between simple_peripheral and a mobile phone can be captured by the connection monitor.
    Looking forward to your reply.
    Deng Junjie
  • Hi Deng,

    It should be possible for the CM to track the complete connection, but it will need to capture the connection establishment fully.

    Best Regards,

    Jan