Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hello Team,
CCS IDE: 20.3.1
SDK: simplelink_lowpower_f3_sdk_9_14_02_15
Car node flashed in: CC2745R10-01 Launchpad having one antenna (initiator)
Key node flashed in: Custom board CC2745R10 having 2 antennas in PCB(reflector)
Distance between these two boards is fluctuating drastically, where car node is kept stationary and key node is moved away. The actual diastance is less than 1m, initially the car node shows 10cm after moving keynode and bringing to the previous position, it is showing 71cm. Sometimes distance is decreasing as keynode is moved farther away and shows more distance if the boards are closer. The results suddenly jumps from 30cm to 250cm, when the boards are staionary.
Note: python script is not used for CS here as shown in the original example of the stack. We modified the stack in car node to automatically connect with keynode and initiate CS procedure with default parameters set.
Please guide me through the changes to be done which can improve the results and reach me if any additional information is required.
please find below sysconfig screenshots of carnode and keynode.


regards,
shreeya