This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: NESB Protocol

Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5, SYSCONFIG

Hi Team,

Posting on behalf of our customer.

I am using the CC2340R5 to build a device-to-device data exchange system, basing it on the NESB protocol. 

The main requirement is for the hub to poll up to five end devices within an 8 ms time slot.
I have successfully implemented a basic TDMA scheme; communication with each end device begins every 1200 µs, and the hub receives an ACK within 5–10 µs. This meets my needs.
The main question is whether I can insert useful data into the end device's ACK.

Regards,

Danilo