This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 and step down converter for Li-ion battery

Other Parts Discussed in Thread: TPS62730, CC2540, TPS62065, TPS62230, TPS62120, TPS780

Hello all,

I am currently working on a battery powered product using the CC2540. I would like to optimize the power consumption. It is recommended in the datasheet to use the TPS62730 step down converter. However, the battery used in my product is a Li-ion battery with a maximum voltage around 4,2V. The TPS62730 cannot be used as it allows input voltage from 1,9V to 3,9V and an absolute maximum voltage of 4,2V. Do you have any solution for optimizing the consumption? Is there an other device working with such batteries?

Thank you for your help.

 Best regards

 CS