This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stack V1.2 UBL Bootloader

Is the source code available for the new USB bootloader? I have downloaded V1.2 of the stack but it appears only to be provided as a .hex with a library file to include in the application to be loaded.

This is a problem for me as my applications do not use the same IO for the USB pull up - it is driven from an IO expander IC instead. 

Thanks

  • Hi Michael,

    If you are referring to the UBL (Universal Boot Loader) there is information in the Universal Boot Loader for SOC-8051 by USB-MSD Developer's Guide found at C:\Texas Instruments\BLE-CC254x-1.2\Documents.

    In any way, both SBL (Serial Boot Loader) and UBL should be included as configurations in the HostTestRelease project (As stated in the release notes)

    Br

  • Hi Nick, yes I am referring to the UBL. I have read the documentation, but I guess the answer to my above question is no- the UBL source is not available?

    If the source is available I would be able to make it work for my projects, but if not I will have to build my own USB bootloader.

    Nick L said:

    Hi Michael,

    If you are referring to the UBL (Universal Boot Loader) there is information in the Universal Boot Loader for SOC-8051 by USB-MSD Developer's Guide found at C:\Texas Instruments\BLE-CC254x-1.2\Documents.

    In any way, both SBL (Serial Boot Loader) and UBL should be included as configurations in the HostTestRelease project (As stated in the release notes)

    Br

  • Hi Michael,

    Correct as far as I know, the UBL source is not available.

    Br