Part Number: CC2745R7-Q1
Hi Forum,
I am opening this new thread to continue this discusstion , the error is coming arbitarily once the channel sounding procedure is enabled. The error is as shown below.

The reasoning behind “GATT writeCB → invoke timer → timer triggers → CS Start” is that the application requirement is to trigger the CS procedure whenever the characteristic value is updated.
I initially tried calling invokeFromContext directly from the GATT write callback, but it did not work as expected. Therefore, I switched to the following approach:
GATT writeCB → start timer → timer timeout handler → invokeFromContext → CS Start
So far, I have only tested this with SDK version 9.14.01.16, because the example I received is a modified version of the car_node example provided by TI. The main modification is that the example is completely self-driven and does not require any host command to initiate the CS procedure.
Regards
Vaibhav