Hi All,
I have a question.
I'm trying to use PAN1323ETU module on Secondary EM header of LM3S9B96 EM2 Expansion Board. But no matter how I config hardware, I can not make it works.
Based on "Stellaris® LM3S9B96 Development Kit USER MANUAL", there's a note :
"NOTE: The secondary EM header should only be used when two EM modules are installed in the
system or when specifically indicated in the EM module’s README First document."
But i don't understand why?
I really appeiciated any help! Thanks!
I'm using the sample bt_spp of dk-lm3s9b96-em2-cc2560-bluetopia.