I just purchased the cc2540 mini dev kit and am trying to learn how to use it.
In the quick start guide it says:
"Select the appropriate flash image by clicking the browse button (marked "…") next to the flash image text field. You will find the flash images in <BLE stack install dir>\Accessories\Hex_Files. Note that there are different files for the keyfob and the dongle."
Yes there are 9 of them. Which one should I use? I’m a beginner. I need to be told everything at this point.
Then it says "You are now ready to run your first Bluetooth® low energy application! For further details, please follow the instructions in the CC2540 Mini Development Kit User’s Guide."
No I'm not ready because it didn't tell me which one to load.
Then in the CC2540 Mini Development Kit User’s Guide it says: "This section describes how to set up the software and get started with the CC2540 Mini Development Kit. It is [wrongly] assumed that the instructions found in [1] (a printed copy of the quick start guide is included with the kit) have already been completed, with both the keyfob and the dongle having been programmed with the latest hex files."
Which ones!
Also, If I ever figure this out, I will need to communicate with the CC2540 with my own program (not BTool) so that the data can be uploaded to a web site. Can anyone point me to an example of how to do that? Isn't this a common need? I didn't see anything like it in the docs.