This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

When will the BLE - iOS sample project be updated?



Hello,

   This is a question for TI. The BLE - iPhone demo is super cool. I installed it and was able to get it to work (well, mostly). After reading the issues that other people have it appears that there are small issues that need to be fixed in it:

1. Needs to be updated for new UUIDs so it works flawlessly with the 1.2+ versions of the examples

2. Crashes on iPad 3

When will this be updated? These seem like they should be fairly quick & easy to have your iOS developer do and will save you lots of time in answering support queries about these two issues.

Thanks,

Derek