I've modified the temperature demo application and am trying to create connections with multiple devices. After turning on the bluetooth and initializing the stack and spp i place the "slave" devices in discovery mode and the have the (1)"master" device start an inquiry. After the inquiry completes i have a list of all (up to 7) "slave devices. I can create 2 acl connections without a problem but when i attempt to connect to the 3rd i will either never get a connection_complete_event response or fail during the SDP process.
Am I running into a limitation of the Mindtree stack? I've attempted to increase various defines in the BT_limit.hj file but have not found the right combination. Changing MAX_SPP_CONNECTIONS to 3 crates a problem in the SDP phase while changing it to 5 causes no connection_complete_event
Any thoughts?
Ryan T.