Is it possible to set up an new forum that deals specifically with Android and/or Apple hardware?
I think most people are really interested in using the CC2540 BLE for cell phone and tablet interfacing.
Unless I'm the only one, but the only reason I purchased the CC2540 was to be able to connect to a cell phone or the iPad.
Information on how to do this is hard to find and useful examples are non existent.
Perhaps most people are using the BLE for Heart rate monitors and thermometers, but I want to be able to use it for plan old control, automation and datalogging. The low energy aspect of it really isn't that important. The CC2540 is an inexpensive way to get connectivity with a multitude of Bluetooth devices. My main goal was to use it as a gateway between a Zigbee network that is doing the automation and controls and the PC, cell phone or tablet. Being able to walk into a factory and check the stats, data or make adjustments to the system on your cell phone, or allowing a customer to see their production in real time on their cell phone or tablet is an incredible selling feature. (I've sold a system that I can't develope yet because of the insane learing curve for BLE!)
It would be nice to have working examples like the Zigbee controllers (light switch control, simple communications, etc). It is easy to see the parallels between Bluetooth and Zigbee for many applications. For those getting started, more help, more code and more explanations are required.
Get some of the Stellaris people to do the documentation.
Not to insult any of the Ti staff, but the Stellaris techs are by far the best in writing understandable documentation for their products. The coding and commenting of the software examples is in a class of its own. Unfortunately, the Stellaris Cortex-M3 was my first Ti microcontroller experience. I became accustomed to having useful examples that you could read through and understand completely. Modifying the example code was very easy because it was so well documented. All this reduced the learning curve from months to days.
From all this, perhaps someone could write a book on the CC2540.
Not one book exist on the interfacing, programming the CC2540 and any device! Sure the technology is new, but everyone getting started has done a search for a CC2540 book and the results come up empty. Ti should publish a book that has useful examples with simple, straight forward explanations. If Ti or anyone else could write a book on the CC2540 similar to the "The Final Word on the 8051" by Matthew Chapman 1994, it would be great!
If I have made any invalid comments, please let me know.
Thanks,