This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some questions about CC2540 & iphone4s

Other Parts Discussed in Thread: CC2540

Dear Ti:

    1,I'm using TI BLE stack v1.2.1, after download programme to the board, the current is between 6-8mA, does this work normal?

     2,in debug mode, can get in the code below just a few times at  beginning,then can not get in again。

          else
         {
              osal_pwrmgr_powerconserve();  // Put the        processor/system into sleep
          }

     3,what is the lowest current when CC2540 & 4S keep in connection state?

     4,when CC2540 & 4s keep in connection, if i run a task that takes long time, the connection was broken, how to avoid this?

     5,can cc2540 be used to transmit files to special application write by me on 4s?

    thanks a lot.