Support,
I have a customer that is trying to run the Penguin accelerator demo. LED1 never switches to solid on to indicate that initialization is complete. I do not have a kit in hand to test this out myself. Could there be a configuration issue at the hardware level?
"If I write the provided version of accl.d43 (the Penguin accelerometer demo) into both boards, the boards will boot up with both LED1 and LED2 blinking. LED1 never switches to solid ON which is supposed to indicate that the initialization is complete and the device is discoverable. Obviously, this means I can’t continue thru the connection phase and onto the application demo."
Thanks,
Tim