This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 Power_Saving with external 32.767KHz Square wave

Other Parts Discussed in Thread: CC2540

Hi:

I try to enable the POWER_SAVING definition in the IAR config.

If I enable the POWER_SAVING, the CC2540 SLAVE will only advertising once.

use an external clock source(square wave of RTC), connect to XOSC32_Q1 (P_4), and use  logic analyzer to check that the square wave is 32.767KHz.

I use the sample code "SimpleBLEBroadcaster" in the BLE stack 1.2.1.

Is there any configuration I missed ??

How to check the POWER_SAVING mode is working???

Thanks.