Other Parts Discussed in Thread: CC2567
- How BT module implement AFH?
- When does the Bluetooth device scan (“sniff”) the frequency space to determine which channels to omit from the hopping sequence?
- Is this done only at the time the devices are paired? Or is it done periodically every "x "seconds?
- What criteria is used to determine whether a Bluetooth channel is to be removed from the hopping sequence?
- Once a channel is removed from the hopping sequence, how long does it stay removed from the hopping sequence?
- Does it stay removed until the devices are re-booted or re-paired? Or does it stay removed until a sub sequence “sniff” of that channel determines the channel is now clear for use? If so, what is the criteria used for denoting a channel as “clear for use”? Or is the channel added back into the hopping sequence automatically after x seconds?