Hi
I've just updated from stack V1.1a to the stack V1.2.1. I used the SimpleBLECentral as starting point for my application.
The new stack works, but with a few problems. If I restart the scanning immediately after a discovery has been finished, a few times in a row, then the stack crashes. If I set a timer to restart scannig automatically, then i need at least a delay of 1second to pervent the crash.Manual over a Uart instruction to restart scanning, I'am not able to reproduce the crash. With stack V1.1a, the problem did not exist.
Any idea what could be the problem?
In the release notes V1.2 is written:
- Multi-role and combo-role support has been enhanced. The BLE stack can now
support simultaneously advertising and/or scanning while in a connection as
either a master or a slave. This allows for a central device to perform
device discovery while in a connection.
Is there a way for scanning other devices in central role while beeing in a connection with one device?
If yes, which command can be used?