Hi everyone,
Currently working on sending text from Stellaris to an Android phone/tablet. I am using the Bluetopia SPP demo application to pair up with the Android phone. So far I have successfully paired.
Here are the console messages:
Client>OpenRemoteServer peter 1
SPP_Open_Remote_Port success.
Client>
atPINCodeRequest: 0xd4206d17e15d
Respond with: PINCodeResponse
Client>PINCodeResponse 1234
GAP_Authentication_Response(), Pin Code Response Success.
Client>
atLinkKeyCreation: 0xd4206d17e15d
Link Key Stored.
Client>
SPP Open Confirmation, ID: 0x0002, Status 0x0000.
Client>
SPP Port Status Indication: 0x0002, Status: 0x000b, Break Status: 0x0000, Length: 0x0000.
Client>
SPP Close Port, ID: 0x0002
But I tried write and it keeps telling me Function Error.
So my questions is this,
1. Do I need a separate application to serve as a bluetooth server on the phone? Or I only need to click the bluetooth settings to send something?
2. If a server application isn't required, are the connection steps wrong?
Any help is appreciated. Thanks in advance.
Harpiebro