This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE simultaneous connection limitations for PAN1326

Other Parts Discussed in Thread: CC2540, CC2564

Hi,

I've read here in the forums that the PAN1326  (MSP430 + cc2564) can maintain up to 8 simultaneous Bluetooth Low energy connections, whereas the cc2540 only supports 4.

The release notes of the cc2540 stack also state other simultaneous connection limitations. i.e. if there is more than 1 connection, the connection interval has to be more 25ms more. 1 data packet per connection. all connection intervals must be a multiple of minimum connection interval.

Are their similar limitations fort the PAN1326?

Rod.