hey,
I have registered two endpoints for a single device .. i.e. registered the device to be a sink as well as source . .
now i want specific device to be connected to the specific endpoint . how this can be done by using bluetopia API's
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hey,
I have registered two endpoints for a single device .. i.e. registered the device to be a sink as well as source . .
now i want specific device to be connected to the specific endpoint . how this can be done by using bluetopia API's
Yes Zahid..
I fixed this issue by registering a endpoint for my device as sink and for source it initiates the paring and bonding procedure so do not require the device to be registered as a source .... later i am able to connect the particular endpoints..
thank you ...
Hi Zahidul,
I was able to locate the SPPLE commands in the demo code. However, I need to send a GATT Read response command, which to a read request from another device. Is there a way to modify the SPPLE demo code to do this especially considering the fact that SPPLE has been emulated using the GATT Profile. If yes, could you please tell how it can be done?
Regards,
Rohit