Hello,
I have bluetooth LE headset connected to may iphone4s.The iPhone is acting as central and headset as peripheral.So how do we get email or sms notification in a bluetooth LE headset from the iphone4s,when a new email or sms arrives.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have bluetooth LE headset connected to may iphone4s.The iPhone is acting as central and headset as peripheral.So how do we get email or sms notification in a bluetooth LE headset from the iphone4s,when a new email or sms arrives.
Hi Anirban,
What is this Bluetooth LE headset, your own design or a purchased one? Depending on if the peripheral device implements server or client functionality, the solution would look different. Could you elaborate a bit more?
Best Regards
Well ok to describe in details i would say that i am having a BLE chip which is used to design a BLE watch.The watch acts as peripheral and gets connected to my iphone4s.Now if a new email or sms arrives in my iphone4s i should be able to send a notification to the watch,which can notify the user that a new email or sms has arrived.How can i achieve this.
Hello Nick,
Can u please suggest any solutions about this matter.
Best Regards
Hi Anirban,
This is very depended on the capabilities on the iOS side, which I cant answer for. Please refer to iOS forums for that. Assuming that you could access this kind of data in the iOS app, it's for example just a matter of writing to a characteristic located in the watch as part of a proprietary profile.
For example, If you are using simpleBLEPeripheral, you could write the information into characteristic 1 (1 byte R/W) of the simpleGATTProfile.
Best Regards