Other Parts Discussed in Thread: CC2540
I have a central and peripheral device that scan, advertise, and connect with each other. The will connect just fine, but I have noticed that once I terminate a connection and then try to reconnect it does not happen. The peripheral begins advertising again, but for some reason the central device is not detecting the peripheral once it has begun advertising again. Is there a setting I need to update in the central device to make it able to detect advertising devices again? What do I need to to so I can reconnect the devices without a power cycle?
Thanks...