This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

paring between 2 bluetooth v4.0 module

Hi Sir/Madam,

We are considering to build our product using TI bluetooth v4.0 chipset. We need to build module first and configure one module as client and the other module master. The client will send data to the master module. The module will be self hosted without host computer. We asked TI China for pairing between 2 modules and the answer is that the module can only pair to a phone or computer with module and running SW/protocol. Is this true that 1 standalone cannot pair to another standalone module?

Coke