This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Anyone see this linker error when attempting OAD in BLE stack v1.3?

Other Parts Discussed in Thread: CC2540

Hello,

I'm trying out OAD on the cc254x.  I've added FEATURE_OAD to the preprocessor defines.

I've also added /profiles/OAD to the library search path.

When building my app or the sensortag app, I see this error:

Linking

Fatal Error[e72]: Segment IMAGE_HEADER must be defined in a segment definition option (-Z, -b or -P)

Error while running Linker.

Did I miss a step?  I'm not sure where IMAGE_HEADER should be defined.

Is there a reference guide to OAD showing how to build for normal flash programming (with OAD enabled), and how to build an image for loading in over the air?

Thanks!

peter

  • Hi Peter,

    There are some steps you are missing. There should be documentation somewhere, I can't find it personally right now.

    However, open up the SensorTag project or SimpleBLEPeripheral project, and select the OAD- build configurations from the dropdown menu at the top of the Workspace pane at the left of the IAR IDE.

    You will then notice some changes..
    Extra preprocessor defines:
    FEATURE_OAD_BIM
    HAL_IMAGE_A
    FEATURE_OAD
    OAD_KEEP_NV_PAGES

     $PROJ_DIR$\..\..\Profiles\Oad added to include path.

    "$PROJ_DIR$\..\..\common\cc2540\cc254x_ubl_pp.bat" "$PROJ_DIR$" "ProdUBL" "$PROJ_DIR$\CC2541DK-Sensor-OAD-ImgA\Exe\SensorTag" added as post-build action. This creates the .bin file used for oad transfer

    $PROJ_DIR$\..\..\common\cc2540\cc254x_f256_imgA.xcl selected as linker file.

    This is true for Img A. There's also Img B, which is placed at another place in flash. The flash is split in three between BIM, ImgA and ImgB.

    To do OAD, you first need
    1) BIM programmed to the device
    2) ImgA programmed to the device using either IAR or Flash Programmer, where you make sure you _DON'T_ erase the flash before programming. This would erase BIM
    3) ImgB .bin file to program OAD. Next time you will need to program ImgA again and so forth.

    To get you started, find CC2541DK_BIM_SensorTagOadImgA.hex in Accessories/Hexfiles under the stack install directory, which is 1 and 2 rolled into one that you can program with SmartRF Flash programmer.

    Best regards,
    Aslak 

  • I forgot to mention that the linker file is where your missing segment is defined.

    Also, in the linker extra output the OAD builds output a .sim file for conversion to .bin. You can also change the normal output to "SensorTag.hex" and format Other->Intel-extended, for programming via flash programmer.

    Aslak

  • Aslak,

    Thank you very much for the full explanation.  I have OAD running and tested using the TI iPhone app.  It seems to work well.

    I do have two followup questions.

    1) Does the OAD service indicate which location it is running from (A or B)?  The iPhone app tells you if you try to update using the wrong side, but the source isn't available yet, so I'm not sure how it can tell.

    2) What is the best way to combine the BIM (BIM_CC254xF256.hex) and Image A into single flashable hex file for production. Should cc254x_ubl_pp.bat be used for that? Are there recommended command line options for this operation?

    Thanks!

    Peter

  • Peter, can you explain which TI iphone app your using to test the OAD?  I didn't realize TI implemented the OAD updater into any of their apps yet

  • Apologies for any confusion.  There was an update today for the TISensorTag app.  It now supports the OAD profile.  It's possible to upload your own .bin files to the app.  I used iExplorer to do this, and placed them in the com.ti.sc.bleweathersample/Documents folder.  I don't know if that's documented anywhere, but I was able to update the firmware of my own application this way.

    Peter

  • Hi Peter,

    1) The source won't be available, but an example OAD app will be made available. If you use Device Monitor that you can find on the sensortag wiki you can enable notifications from OAD Image Notify and write first 00 and then 01 to the characteristic. If image A is running, you will get a sensible notification back after writing 00, otherwise from 01. The response is <image_id><image_len><user_id>, where the LSB of image ID tells you A(0) or B(1), and the 7 LSB are the version you have set.

    Currently the Sensortag App looks for 0x41 (A) or 0x42 (B) in the user id, which is a bug that will be fixed.

    2) For me it worked to simply concatenate the BIM hex file and the Image A hex file in a text editor or use the command line with type "bim.hex > superhex.hex" and "type imga.hex>>superhex.hex" in dos prompt. Otherwise you could potentially use flash programmer to read back the image that you have flashed to the device. Note that this last solution may be a bad idea, as calibration data could have been written to flash already by the device by the time you read back flash - data which may not be correct for another device.

    Best regards,
    Aslak

  • Hi Aslak,

    Thanks so much.  That's just what I needed to know to keep things rolling.

    Cheers,

    Peter

  • Hi guys,

    I have a problem same as via IAR build SensorTag occur IMAGE HEADER fail.

    Question 1,

    I want use SensorTag main function build hex include OAD profile , not ImageA/ImageB to build.

    when I

    1. Select Project->OptionsC/C++ CompilerPreprocessorDefined symbols and add 

      =>       FEATURE_OAD

    IAR will pop error message say IMAGE HEADER fail

    Do we have any resolution?  

    Question2,

    SensorTag provide ImageA and ImageB difference for what? 

    Thanks a lot

    Ben