Hello,
I want to create a ble application that can make the device to act as client and server at the same time. It
should be able to maintain one connection with a client device while itself acts as a client in a second
connection. Does that make sense?
Is it possible to maintain two connections at the same time if the device should act server and client at the
same time on ti devices?
Best regards,
Patrik Hillbo