Hi,
I am a newbie in RF. I am using a Panasonic PAN1323ETU bluetooth module. Does the antenna orientation effect the range of bluetooth? Should there be 2 different antenna orientations for polarizations?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am a newbie in RF. I am using a Panasonic PAN1323ETU bluetooth module. Does the antenna orientation effect the range of bluetooth? Should there be 2 different antenna orientations for polarizations?
Thanks.
Hi Gautam,
Yes, the antenna placement has an impact on performance. For guidelines regarding this topic, please refer to the PAN13xx Datasheet.
http://processors.wiki.ti.com/index.php/CC256x_Modules#Panasonic_Modules
Regards,
Miguel
Hello,
This is an area that interests me as well. I've been looking at chip antenna radiation patterns, which are also indicative of sensitivity. In particular, I'm interested in transmit/receive performance within a 3D space.
TI has some information on antenna performance that you may find useful in extrapolating the effects of orientation.
See: http://www.ti.com/lit/an/snoa519a/snoa519a.pdf for an example.
Another [non-TI] example can be found at www.pulseelectronics.com/download/2964/w3008_w3008cpdf
Best wishes to you.
Thanks Tim. I had gone through that earlier. I understood it to some level but not much. The radiation pattern shows that it covers most areas but I am not sure whether I have to consider polarization as there is no notes on it. Am I missing something? The device I am designing is a device stuck to a body whose orientation can be anything.
Just to simplify things, if you have two antennas of a particular type - in this case chip antennas mounted on circuit boards - and these antennas are physically oriented the same way (i.e. their tops point "up" and each of their other corresponding faces are similarly oriented) then their polarizations are matched. For antennas on mobile devices, polarization is useful as a measurement reference, but since the devices orientation is uncontrolled then it is useful (to me, at least) to consider best & worst cases. This is one reason for looking at the radiation patterns for different antenna geometries - to see if they have any potentially troublesome "dark sides."
Your use case sounds something like a biometric telemetry application in which one or more devices attach to the body and collect data describing things like temperature and heart rate and then transmit this data to one or more other devices (likely also in close proximity to the same body). In such a case you may have some control over the sensor antenna orientation, but the receiving device may be in any orientation. If you don't have an omnidirectional radiation pattern then you may discover that, under some conditions, you don't have a reliable signal at either or both sides of the "conversation."
This may not be a problem with Class II devices, which can transmit signals well beyond the range of a physical Personal Area Network (10 meters is beyond my own reach). With such a transmit power level you may not have any real problems, even when antennas are not optimally oriented.
Another factor in your favor is that people tend to be around things that reflect RF signals. Even if you have a master and a slave located on opposite sides of a very large person who, for some reason, absorbs abnormally high amounts of 2.4GHz signals, nearby objects may reflect enough energy to allow the system to work fine anyway.
Ultimately, you can do some empirical testing out in a field (or in a wooden boat on a lake...or something) and see what happens when you move the radios around with respect to each other. I suspect that you are okay if you are using an off-the-shelf Bluetooth module.
Lastly, if you are developing a proprietary system (and not creating "dongles" that communicate with a 3rd party device, such as a smart phone), then you might consider using a Body Area Network rather than a radiated energy system. I don't know what your application is or what bandwidth you might need, but body area networks can be a very reliable and low energy means of shipping data among points on the human body.
Best wishes.
Thanks for taking the timeout to write a detailed reply.
I have some doubts below:
Tim Bergin said:Just to simplify things, if you have two antennas of a particular type - in this case chip antennas mounted on circuit boards - and these antennas are physically oriented the same way (i.e. their tops point "up" and each of their other corresponding faces are similarly oriented) then their polarizations are matched. For antennas on mobile devices, polarization is useful as a measurement reference, but since the devices orientation is uncontrolled then it is useful (to me, at least) to consider best & worst cases. This is one reason for looking at the radiation patterns for different antenna geometries - to see if they have any potentially troublesome "dark sides."
Your use case sounds something like a biometric telemetry application in which one or more devices attach to the body and collect data describing things like temperature and heart rate and then transmit this data to one or more other devices (likely also in close proximity to the same body). In such a case you may have some control over the sensor antenna orientation, but the receiving device may be in any orientation.
It is exactly a biometric telemetry application. I didn't get as to how to how I would have control over the antenna. The data collection (or receiving) master might be a mobile device or a station mounted beside his bed. The patient might be oriented anyways either in sleeping horizontal position or slanted or vertical. In fact even both the sending and the receiving device can be in any orientation.
Tim Bergin said:If you don't have an omnidirectional radiation pattern then you may discover that, under some conditions, you don't have a reliable signal at either or both sides of the "conversation."
If I have an omnidirectional radiation pattern would I be getting a good signal in all orientations? For eg for wifi I thought its usually vertically polarized or is there somethingabout the chip antenna's I am missing where polarization does not matter?
Ultimately, you can do some empirical testing out in a field (or in a wooden boat on a lake...or something) and see what happens when you move the radios around with respect to each other. I suspect that you are okay if you are using an off-the-shelf Bluetooth module.
Yup. I should do this. When you say a field or a lake it means that there shouldn't be any reflections(eg: off the walls) right?
I was making an assumption (which is often a dangerous thing to do) that the sensor, or sensors, would be attached or worn in a limited range of orientations. As an example, there might be a chest band that keeps a sensor pack that collects heart signal (i.e. simple rate or full EKG), respiration rate, local skin temperature, etc., in intimate contact with the patient / subject. The means of attaching such a package might limit the potential range of antenna orientations with respect to the patient. However, since you may have a master - or receiving / processing unit - that may be realized in the form of a 3rd party device (such as a smart phone), then you can't predict how the antennas will be oriented with respect to each other. All bets are off.
Since I don't have the luxury of an anechoic chamber and a full suite of spectrum and power measurement instruments anymore, I take a less sophisticated approach to getting things into a safe operating range. In your case I might begin by looking at the reported behavior of your antennas and look for the orientation that provides the poorest performance (in three dimensional terms...at what azimuth & elevation is the antenna least sensitive?).
For an example, take a look at this spec: http://www.pilkor.net/pilkor/www/b/chip_antenna_ant3216_b273haa_en.html
This antenna has relatively uniform performance around the Y axis, yet has some reduction in performance around the Z and X axes at roughly 240 and 300 degrees. In my "shade-tree mechanic" tests, in which I would try to develop a more subjective (less objective) sense of performance, I would attempt to orient my radios such that they were each in the least sensitive orientation - and then I would place an absorbing body (such as my own) between then and check my bit-error-rate.
I have yet to see a truly omnidirectional antenna, particularly once the antenna is packaged with other junk and then placed into a real-world environment. However, you can look at the antenna specs and try to settle on an antenna that provides an acceptable and relatively uniform performance around all axes. That, at least, is a starting point. You are right about the WiFi antennas and this is why you will see MIMO routers with their three antennas oriented normal (at 90 degrees) to each other. The roughly toroidal radiation patterns of each antenna overlap to create a 3D volume with fewer discontinuities.
As to the field or lake comment, you are correct and I meant that you should try to get away from confounding factors, such as reflections and other signal sources, if & when you do your testing.
In the real world, I've seen guys with fantastic instruments get outperformed by the simple judgement of other guys who have developed a strong intuitive sense of how things work. While you can't eliminate all potential sources of signal failure, at least you can reduce the risk through some basic benchwork. You seem to have a good sense of what's going on and it's helpful that you are willing to do the due dilligence work. This will help you in the future - it will help you to develop an intuitive sense of what will work.
Best wishes to you.
Correct me if I am wrong but in the TI application note at Page 5 and Page 6 the radiation looks somewhat spherical as the elevation cut and the azimuth cut does not have any NULL beam right (which is what I am worried about)? The elevation cut looks particularly nice with a slight bump between 120 and 180. In the pilkor chip antenna link are they re-orienting the antenna in each of the 3 radiation patterns?
NULL beam, as in transmit power / receive sensitivity dropping to zero at some angle? No, it doesn't get that bad, but the pattern doesn't become spherical, either. I've never seen a single antenna pattern that is spherical, particularly after the antenna and PA are bundled into a package. I have a need for a relatively spherical pattern within a large volume and will likely need to use more than one BT radio & antenna (I'm looking closely at this).
The elevation and azimuth graphs also don't tell the full story - I prefer the 3D renderings (such as http://www.antennawizards.com/images/M2M_pattern.PNG ), which are created through modeling and/or painstaking measurements. Note that the colorful image is for a planar inverted F antenna, which are sometimes used for Bluetooth.
The Pilkor example is just one more step above the elevation-azimuth plots in that it provides more information, though it is not as complete a visualization as is a 3D plot.
I don't think you'll have a functional dead zone (meaning that you can't ship data reliably) if you are using a Class II to communicate within a purely personal space (literally, a PAN with all devices within arm's reach). However, if you have a life safety application and need to be worried about black swans then it would be a good idea to bring in a skilled RF engineer. In such a case it's worth the money to have an expert looking over your shoulder.
For fun, do a Google image search on phrases like "bluetooth chip antenna radiation pattern" and see how things vary.