This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TimeApp BTool



Hello,

I’m running two RF05 one with TimeApp and one with BTool. Scan and establishing works fine with BTool. Display shows connected.

How can I set the time with BTool?

Thanks and best regards,

 

Holger

  • Hello,

    I assume you are trying to use the BTool as the Time Server, and trying to emulate that BTool will deliver the new time when it is adjusted, correct?
    Here is the Time Profile document, and take a look at what scenario you want BTool to emulate:

    Time Profile: https://www.bluetooth.org/docman/handlers/downloaddoc.ashx?doc_id=241874

    You can use the Read/Write functionality of BTool with the correct characteristics.

    LPRF Rocks the World

  • Hello,

     Note: I use BTool Application v1.30d

    I fall back to TI demo SWRU301A page 18. After scanning and establishing I can read using characteristic UUID  “F1:FF” and get handle (0x0022) and value (01). Everything for reading is fine.

    As described for writting, with handle 0x0022 and value 7 the display shows “Char 1: 7”, but I get at the end always an error? (see below)

        

    29] : <Tx> - 10:53:47.765

    -Type                      : 0x01 (Command)

    -Opcode                  : 0xFD92 (GATT_WriteCharValue)

    -Data Length           : 0x05 (5) byte(s)

     ConnHandle           : 0x0000 (0)

     Handle                   : 0x0022 (34)

     Value                     : 07

    Dump(Tx):

    01 92 FD 05 00 00 22 00 07

     

    ------------------------------------------------------------------------------------------------------------------------

    [30] : <Rx> - 10:53:47.781

    -Type                      : 0x04 (Event)

    -EventCode             : 0xFF (HCI_LE_ExtEvent)

    -Data Length           : 0x06 (6) bytes(s)

     Event                     : 0x067F (GAP_HCI_ExtentionCommandStatus)

     Status                    : 0x00 (Success)

     OpCode                 : 0xFD92 (GATT_WriteCharValue)

     DataLength            : 0x00 (0)

    Dump(Rx):

    04 FF 06 7F 06 00 92 FD 00

     

    ------------------------------------------------------------------------------------------------------------------------

    [31] : <Rx> - 10:53:47.921

    -Type                      : 0x04 (Event)

    -EventCode             : 0xFF (HCI_LE_ExtEvent)

    -Data Length           : 0x06 (6) bytes(s)

     Event                     : 0x0513 (ATT_WriteRsp)

     Status                    : 0x00 (Success)

     ConnHandle           : 0x0000 (0)

     PduLen                  : 0x00 (0)

    Dump(Rx):

    04 FF 06 13 05 00 00 00 00

     

    ------------------------------------------------------------------------------------------------------------------------

    [32] : <Error> - 10:54:27.782

    Message Response Timeout

    Name = GATT_WriteCharValue

    Opcode = 0xFD92