Hello:
I have the CC2540_MINIDK kit, and want to Tx/Rx data using UART DMA in Port0 (P0.2 and P0.3). Using the configuration settings, I able to DMA Rx bytes correctly. But when I trying to Tx bytes by calling HalUARTWrite(...), the DMA UART Tx doesn't send out bytes. I put the digital scope on P0.2 and P0.3 and don't see Tx occurs.
Can you help me to configure the CC2540_MINIDK GPIO to have the UART DMA Tx output correctly?
Thank You
Mike
------------- My UART Configuration ----------------
INT_HEAP_LEN=2900
HALNODEBUG
OSAL_CBTIMER_NUM_TASKS=1
HAL_AES_DMA=FALSE
HAL_DMA=TRUE
xPLUS_BROADCASTER
HAL_LCD=FALSE
HAL_LED=TRUE
HAL_UART=TRUE
CC2540_MINIDK=TRUE
DEBUG_TURN_ON
POWER_SAVING
#define SBP_UART_PORT                  HAL_UART_PORT_0
//#define SBP_UART_FC                    TRUE
  #define SBP_UART_FC                    FALSE
#define SBP_UART_FC_THRESHOLD          48
#define SBP_UART_RX_BUF_SIZE           128
#define SBP_UART_TX_BUF_SIZE           128
#define SBP_UART_IDLE_TIMEOUT          6
#define SBP_UART_INT_ENABLE            TRUE
//#define SBP_UART_BR                   HAL_UART_BR_115200 
//#define SBP_UART_BR                   HAL_UART_BR_57600 
//#define SBP_UART_BR                   HAL_UART_BR_38400
//#define SBP_UART_BR                   HAL_UART_BR_19200
#define SBP_UART_BR                     HAL_UART_BR_9600
void serialAppInitTransport( )
{
  halUARTCfg_t uartConfig;
  
  // Initialize UART variables
  g_pktIndex = 0;
  // configure UART
  uartConfig.configured           = TRUE;
  uartConfig.baudRate             = SBP_UART_BR;
  uartConfig.flowControl          = SBP_UART_FC;
  uartConfig.flowControlThreshold = SBP_UART_FC_THRESHOLD;
  uartConfig.rx.maxBufSize        = SBP_UART_RX_BUF_SIZE;
  uartConfig.tx.maxBufSize        = SBP_UART_TX_BUF_SIZE;
  uartConfig.idleTimeout          = SBP_UART_IDLE_TIMEOUT;
  uartConfig.intEnable            = SBP_UART_INT_ENABLE;
  uartConfig.callBackFunc         = funcSerialPacketRx;
  // start UART
  // Note: Assumes no issue opening UART port.
  (void)HalUARTOpen( SBP_UART_PORT, &uartConfig );
  return;
}