Hi
I am not able to receive data on UART0 of cc2540
I am trying to receive data on Win Xp based hyperterminal from CC2540EMK
I am using the following configuration for communication, not able to locate the problem
checking serial packets on ( Rx on P0.2 & Tx on P0.3) (ie. pin 7 - Rx & pin 9 TX of P1 of cc2540emk)
#define SBP_UART_PORT HAL_UART_PORT_0
//#define SBP_UART_FC TRUE
#define SBP_UART_FC FALSE
#define SBP_UART_FC_THRESHOLD 48
#define SBP_UART_RX_BUF_SIZE 128
#define SBP_UART_TX_BUF_SIZE 128
#define SBP_UART_IDLE_TIMEOUT 6
#define SBP_UART_INT_ENABLE TRUE
halUARTCfg_t uartConfig;
// configure UART
uartConfig.configured = TRUE;
uartConfig.baudRate = SBP_UART_BR;
uartConfig.flowControl = SBP_UART_FC;
uartConfig.flowControlThreshold = SBP_UART_FC_THRESHOLD;
uartConfig.rx.maxBufSize = SBP_UART_RX_BUF_SIZE;
uartConfig.tx.maxBufSize = SBP_UART_TX_BUF_SIZE;
uartConfig.idleTimeout = SBP_UART_IDLE_TIMEOUT;
uartConfig.intEnable = SBP_UART_INT_ENABLE;
uartConfig.callBackFunc = NULL;//PollSerialPort;
(void)HalUARTOpen( SBP_UART_PORT, &uartConfig );
Am i checking data packets on a wrong port?
Not able to identify what is going wrong. Please help
BR
Gautam