This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please suggest Bluetooth Solution for a Game console

Hi Everyone,

I need to design a wireless Game console which is going to have:

1. Stereo Audio output 

2. 2x Analog Sticks + 12 to 16 Inputs for various Push Buttons

3. A Full Qwerty keypad

4. USB interface for firmware update (Optional)

5. Bluetooth Connectivity (Low energy preferred)

Can someone please suggest single chip / Module based solution that is capable of providing Bluetooth connectivity which is programmable. If there isnt any single module / single chip solution that fits my need then i can consider using a microcontroller (with good support for Bluetooth profiles).

For QWERTY keypad i understand that i may need an external IO expander chip on SPI or I2C interface. 

Regards