This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it possible send the information of two or more sensors to only one phone via bluetooth?

Other Parts Discussed in Thread: CC2540

Hello

We'd like to know if it is possible to use only one smartphone to receive the information of several of these sensors. Is it possible?

Thanks

  • Hello Juan,

    Yes it is possible. You can use one smartphone and receive information from an infinite number of CC2540/41 devices.

    The easiest way would be to give each device a unique name like "Sensor_xxx" and have the smartphone sequentially connect to each one, read the data and then connect to another.  There are other methods as well.

    Search the forum to find other ways.

    Thanks,

    ----Mark this answer as VERIFIED if you are satisfied.