Hi, hand built 3 transmitters using CC2540. Three because I thought I had a short from pin 40 to pin 41, the ground pad on the ic base. It was only when I checked on an unsoldered CC2540 that pin 40 is connected to the ground plane. On all the application schematics there is nothing to show that pin 40 is connected to pin 41. On the schematic pin 40 is shown with a 1uf decoupler to ground. Can anyone confirm that this is the case i.e. that pin 40 is connected to pin 41 on the die and if so why the 1uf decoupler. Also - T.I. an explanation on the schematic would be helpful to save hours of frustration and wasted time.