Other Parts Discussed in Thread: CC2541
Hi
I have a couple of questions on BLE:
1) For the BLE using CC2541 is it possible to connect up as a mesh? If not, I believe star is possible, yes? Is there any max number of nodes in a star or mesh configuration?
2) For BLE, our undersatndning is there are 49 channels used, 3 for advertising and after which there would be a hop to a not busy channel. However, when using two EVB, first board establish communication and continuous transmission. When we get the second board to establish communication, it goes to the same channel as the firs board, instead of the other free 36 channels. Is this a fair observation.
Ivan