This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bluetooth app in iOS 6 Simulator

Hi,

I'm trying to run TI's SensorTagEX sample application for iOS. On an iOS 6 device, it runs fine. It also runs fine on the iOS 5 Simulator using the Cirago Bluetooth LE adapter. However, it does not run on the iOS 6 Simulator. The app simply fails to connect. It's frustrating because testing code on the simulator is so much faster, and my code happens to require iOS 6. And as I said, it definitely works on the iOS 5 Simulator. Is this a known issue with Apple's iOS 6 Simulator? Thanks,

Trevor