I understand that the stack is currently limited to 3 slaves connected to a master at a given time. I also understand the current throughput for a given connection to be limited to roughly 5.9kbytes/sec. When I have all three slave connected can I expect each slave to be able to achieve roughly 5.9kbytes/sec resulting in a total network throughput of roughly 17.7kbytes/sec? Or is the total network throughput limited to 5.9kbytes/sec which means each slave is only achieving roughly 2kbytes/sec?