Other Parts Discussed in Thread: CC2540, CC2570, CC2571, CC2564, CC2567
Hello,
What profile should I use if I want a group of transient devices to join a master and react for an event?
Example: 10 people wearing BLE hats walk to the same area and when someone press a button the hats get signal to flash LEDs .
In this case the button is the master and the hats are the slaves.
There is no confirmation needed, so Broadcast works fine.
Am I constrained to only 3 slave devices in broadcaster mode? How can I word around it?