Other Parts Discussed in Thread: TPS62730, CC2541
In TPS62730 datasheet(SLVSAC3C-MAY 2011- REVISED DECEMBER 2012), it mentiones"Once the device is turned from ultra low power bypass mode into buck converter operation for a RF transmission, all the internal circuits of the regulator are activated within a start up time tStart of typ 50µs. During this time the bypass switch is still turned on and maintains the output VOUT connected to the input VIN. Once the DC/DC converter is settled and ready to operate, the internal bypass switch is turned off and the system is supplied by the output capacitor and the other decoupling capacitors. The buck converter kicks in once the capacitors connected to VOUT are discharged to the level of the nominal buck converter output voltage." in page 14. My question is that in this period from "bypass" mode to "on" mode, or in the reverse direction, the output voltage of TPS62730 changes ,and in the meantime the CC2541 still works and also with its inner processor 8051, will the supply voltage vary cause some uncontrollable errors or states that takes place in CC2541. thanks!