I am trying to find more information on the power saving modes. Will someone please point me in the right direction?
My problem is that the battery on my peripheral device is only lasting about 4 weeks and I need it to last much longer., (the load being pulsed on the battery by the radio when transmitting and receiving is not helping anything either). I have a peripheral device powered by a coin cell battery, once connected to my central device it stays connected 24/7. I would like to determine when the device is inactive and then force it to sleep so I am not consuming as much power. The Tx power on my peripheral device is set to -6 dBm.
Can the device go to sleep and still stay in a connection?
Do I need ternimate my connection and then sleep then reconnect after waking up the device?
What is recommended?
Thanks...