This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"Central and Broadcaster" example or "Peripheral and Observer" example in one module.

Hi All,

I'm looking for example of:

"Central and Broadcaster"  example or "Peripheral and Observer" example in one module.

As a starting point for my project.

I tried to build such a project myself, but i cant understand if the combined profile should be used in the same task OR

to  make two different tasks for each profile?

Is there a conflict on the GAP when trying to start to tasks with different profiles?

Is it logical to call 'GAPRole_StartDevice' from two different tasks?

Any help, will be appreciated.

Tn'x in advance

Meir Lebel