Other Parts Discussed in Thread: CC2540
Hi,
I am using the SensorTag hardware with the sample SensorTag application modified with the Data throughput examples:
http://processors.wiki.ti.com/index.php/CC2540_Data_Throughput
I am sniffing the BLE packets with TI's SmartRF packet sniffer.
The setup is then:
- 1 SensorTag as BLE peripheral
- 1 CC2540 USB dongle as BLE Central
- 1 CC2540 USB dongle as sniffer
During the transfer, I can that L2CAP packets are transmitted several times (0x1EE data packet in next picture) without seeing any problem in the packets. Can anybody explain me why these packets are retransmitted?
Best regards,
Greg