I used LMX9838 bluetooth module in my project.I connected 3 LMX9838 together.They are working well.Now,I used a bluetooth in the computer to connect the master LMX9838. The computer can found this LMX9838 , pairing and established a link. The computer can display this link is SPP mode and COM port is COM8. But when I use real-term serial software to test these link.It appear the 'Apro exception' error. But it worked well when I establish a link with point to point . Could you help to solve this problem. BTW.What port will the LMX9838 use when the pairing is successful and how can I check this link. Thank you so much