This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does BLE112 of bluegiga work with SmartRF Packet Sniffer?

Other Parts Discussed in Thread: CC2540, CC-DEBUGGER

Can I use BLE112 as a btle packet sniffer?

I wrote TI SmartRF Packet Sniffer's recommended firmware: sniffer_fw_cc2540.hex or sniffer_fw_cc2540_usb.hex 

using CC-Debugger, but both doesn't work with following error.

"Failed to set debugger profile", "Not able to start the sniffer. Try to upgrade USB firmware."

The firmware version shown in SmartRF Flash Programmer is:

EB firmware ID: 05CC 
EB firmware rev: 0041

Or, does BLED112 (bluegiga's usb dongle) work as a packet sniffer?