This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564 - MSP430 -Bluetopia

Other Parts Discussed in Thread: CC2540, CC2564, MSP430F5438

Hi all,

I have previously worked on CC2540/41, which contains 8051 to implement BLE. But the CC2564 is just a controller(HCI ) ? is it integrated with Panasonic's Radio module to form  PAN1326 which then can be connected to the MSP430F5438 (Host Processor as mentioned in the Figure below) ?.On the Host Processor ,Stone street's one Bluetopia is running, SS1 stack here is ported  to run on MSP430. Both the HCI layers will speak to each other through the UART lines ? Please help to understand the scenario ?