Hi,
I have read all the Wiki pages and I have these questions and I am wondering if I could get the answers. I have purchased the kit with two target boards and USB device.
1. What is exactly already pre-downloaded on the target boards? Is it the accelerometer project from MindTree EtherMind™ Bluetooth® Stack (which you do not support any more). If this is the case please elaborate (I feel it is the case as it comes with Penguin example), if not I would need to have the CCS/IAR workspace/project that are on these target boards.
2. I need to have a simple project just sending data through Bluetooth or LE from the target board with battery to the one with USB. The demos on http://processors.wiki.ti.com/index.php/CC256x_MSP430_Bluetopia_Basic_Demo_APPS are for the experiment setups that I do not have and their size is not acceptable by CCS (large). So I need just a simple communication project for EZ430-RF256x kit as a template.
3. Is there any way I know what is already on the target boards (both of them) so that I have the source project to change/develop.
Thanks and these information are not on the forums, wikis, etc.
Mehran