Clarification needed for package dimension.
Below a marked up copy of Fig 16 from the TI QFN PCB Guidelines doc (SWRA420), which indicates dimensions A, B and C – these have been inferred from the Package Dimensions (Fig 15).
Altium IPC Footprint Wizard was used to generate a Footprint for this part with correspondence on dimensions A and B, but contention on dimension C – the Altium IPC Footprint Wizard indicates that dimension C should be set to 3.925 mm, versus a Package derived value of 3.8 mm. I believe the 3.925 mm dimension is correct for actual assembly of this part - could you please confirm?