Hi Everyone,
I have finished my LMX9830 BT implementation, and it all looks pretty smick. I have configured the LMX9830 to load its setup into NVS from a SPI Flash (a
M95640-S). The idea is to configure the device at power on saving the need to do so from my small MPU.
Would anyone have a ROM dump they could share with me showing the bytes used to configure the LMX9830 at power on? Id like to be able to understand the structure of the configuration ROMs data so as to create my own. Something showing whats required, at which address locations would be great.
Many thanks,
Steve